Supporting the Transition away from Fossil Fuels with the Power of Electronic Components
What Are the Conditions for Increasing the Efficiency of Power Conversion and Motor Drives and for Expanding the Use of SiC and GaN Power Semiconductors?
There is a move to update the base material of devices from Si to SiC or GaN in the power semiconductor field to accelerate the pace of efforts to achieve carbon neutrality. We explain here what technological advances are needed in peripheral components such as capacitors and inductors to maximize the effect of that update.