Capacitor
Tantalum capacitors are often used as the capacitor connected to the power line of PA (= Power Amplifier) for GSM on smart phones. In this report, we evaluate replacing the tantalum capacitor (Ta-Cap) with a ceramic capacitor.
We purchased a smartphone and evaluated it. The circuit of the battery line, which is the analysis of our own, is shown in the figure below. A Ta-Cap is connected near the power line of the PA for GSM.
The proposal is illustrated below. We selected the low acoustic noise Ceramic capacitor "ZRB series" as replacement. As you can see, the mounting space is reduced by 50%.
C1: Ta-Cap 100uF/1206size × 1pcs → Low acoustic noise ceramic capacitor 22uF/6.3V/0603size × 2pcs
We measured the following properties before and after replacement.
The value of the capacitor that is connected to the PA power line affects signal quality. Therefore, it is necessary to test the communication characteristics.
If the impedance of the power line changes, noise will change. Therefore, it is necessary to test the power line voltage fluctuations of the PA.
The PA for GSM is operated by a burst audible frequency (217Hz) cycle. Therefore, an evaluation of acoustic noise is required.
Communication characteristics and voltage fluctuation were tested by the measurement system below.
The communication characteristics meet the standard for GSM.
The communication characteristics meet the standard for GSM.
The noise of power line is reduced 7–8%.
The noise of power line is reduced 14–22%.
Acoustic noise is measured as sound pressure level (SPL) by the measurement system below.
SPL is equal to the initial. (There is no significant difference.)
We evaluated replacing the Ta-Cap that is connected to the power line of the PA for GSM with a ceramic capacitor. In the evaluation, we tested (1) the communication characteristics, (2) the voltage fluctuation, and (3) acoustic noise.
The communication characteristics are equal to the initial and meet the standard for GSM.
Voltage fluctuation is reduced 7–22%.
Acoustic noise level is equal to the initial.
Advantages of replacing the Ta-Cap with a ceramic capacitor
Ceramic capacitors have low ESR and low ESL characteristics. Therefore, the impedance of a ceramic capacitor (22uF/6.3V/0603size) is smaller than that of a Ta-Cap (100uF/6.3V/1206size) over 100kHz range. Thus, the ceramic capacitor has a better noise suppression effect at a high-frequency range.
Temp. rise level is lower than Ta-Cap. due to low ESR.
Ceramic capacitors have high breakdown voltage.
We demonstrated the evaluation result of replacing the Ta-Cap with a ceramic capacitor, and the benefits of using a ceramic capacitor.
Evaluation for replacement
Benefits of using a ceramic capacitor
Proposal
C1: Ta-Cap 100uF/1206size × 1pcs → Low acoustic noise Ceramic capacitor 22uF/6.3V/0603size × 2pcs
Replacement parts number: ZRB18AR60J226ME01
Contact your local Murata sales rep for further support.