Main image of What Is mmWave Radar? Principles and Usage Examples

What Is mmWave Radar? Principles and Usage Examples

In general, radar (originally an acronym for "radio detection and ranging") is a device that detects the distance to a target and its direction by emitting electromagnetic waves (radio waves) toward the target and then measuring the radio waves that are reflected back. Accordingly, mmWave radar refers to radar that uses milli-waves as its radio waves.
Compared to infrared rays and cameras, mmWave radar's detection capabilities do not decline even in adverse weather conditions such as rain, snow, and fog. Moreover, in addition to the distance to a target and its direction, it can also detect the target's speed of movement. Here, we take a look at the detection principles, usage examples, and future potential of mmWave radar, which possesses these characteristics.

1. What Are Milli-waves?

Figure 1 shows the range where milli-waves (also referred to as "mmWaves") fall within the classification of radio waves. In general, milli-waves refer to radio waves with frequencies from 30 GHz to 300 GHz and wavelengths from 1 mm to 10 mm*1. They are called milli-waves because their wavelengths are measured in millimeters (mm).

*1 In fact, there is no strict definition of the frequency range of milli-waves. For example, the 26 GHz and 28 GHz bands, which are now being allocated to 5G communications across the globe, are also treated as milli-waves.

Classification of electromagnetic waves by frequency category
Figure 1: Classification of electromagnetic waves by frequency category

The characteristics of milli-waves include strong directivity and the ability to secure a wide frequency bandwidth. Table 1 summarizes these characteristics.

Table 1: Main characteristics of milli-waves
DirectivityAs shown in Figure 1, the frequency of milli-waves is close to that of light. Therefore, milli-waves exhibit
strong directivity similar to light. This means we can say the following about milli-waves.
a-1: The signal strength is attenuated by shielding from obstacles such as walls or in the event of
extremely adverse weather conditions.
a-2: Milli-waves are not suited to long-range communication due to a-1.
a-3: Interference with nearby milli-wave systems is less likely to occur in short-range communication.
a-4: Milli-waves can penetrate fabrics, resins, and other materials.
Frequency
bandwidth
The milli-wave bandwidth is an unexplored domain. It is a frequency band for which there is still little
demand. This means it is possible to secure a wide frequency bandwidth.
(Currently, most frequency domains below a few GHz are already being used. Accordingly, securing
bandwidth is subject to the radio laws and business constraints.)

Wider frequency bandwidth leads to higher accuracy in distance detection in radar (see section 2). Therefore, we can say that frequency bandwidth is an important specification. Furthermore, wider frequency bandwidth leads to faster communication speeds in mobile communications or similar ("Time and Frequency Domains - The Basics of Digital Communication").

2. mmWave Radar Methods and Characteristics

As we mentioned at the beginning of this article, mmWave radar is a device that detects the position of a target by emitting milli-waves toward it and then receiving the waves that are reflected back. It can detect objects within a range of up to approximately 300 meters.
Currently, the frequency bandwidths available for low-power radar are the 24 GHz*2, 60 GHz, 76 GHz, and 79 GHz bands. Technical requirements have been specified for each of these. Among them, milli-wave bands (60 GHz, 76 GHz, and 79 GHz bands) have a wide bandwidth. This enables highly accurate detection.
The leading mmWave radar methods are the pulse method and the FMCW method*3. Table 2 describes the characteristics of these methods.

Table 2: Pulse method and FMCW method

Pulse Method

FMCW Method

This method involves emitting extremely short pulses of
tens of nanoseconds to several microseconds toward a
target, then determining the distance to the target, its
speed, and its angle from the round-trip time until the
reflected pulse is received (Figure 2). The detection
principle is uncomplicated. Moreover, the circuit
configuration is simpler than that of the FMCW method.

This method involves emitting a transmitted wave*4
obtained by modulating the frequency of a continuous
wave toward a target, then determining the distance to
the target, its speed, and its angle from the difference
between the transmitted wave and the reflected wave.
It is also possible to measure the speed of movement
relative to the target (Figure 2).

Illustration of target detection using mmWave radar
Figure 2: Illustration of target detection using mmWave radar

*2 24 GHz band: The wavelength of the 24 GHz band is 12.5 mm. This is not included in the 10 mm to 1 mm range defined for milli-waves. Therefore, milli-waves in the 24 GHz band are called "quasi-milli-waves."

*3 FMCW stands for "frequency modulated continuous wave." It refers to a method that uses a continuous wave whose frequency has been modulated.

*4 Figure 3 shows an image of a transmitted wave in the FMCW method. This wave is sometimes called a chirp waveform.

Image of a chirp waveform
Figure 3: Image of a chirp waveform ("chirp" here refers to the chirping sound of a bird)

3. Configuration and Detection Method of FMCW mmWave Radar

There are many mmWave radar methods. Nevertheless, most are advanced versions of the FMCW method. Accordingly, we will explain below the configuration of an FMCW mmWave radar and the general principle for detecting targets. Although the configuration is simple, it can acquire complex information such as distance, speed, and angle.

Target detection using mmWave radar
Figure 4: Target detection using mmWave radar

<mmWave radar configuration>
Synthesizer: Generates the radio waves in the milli-wave band to be transmitted (transmitted waves)
Tx antenna: Emits the transmitted waves
Rx antenna: Receives the reflected waves
Mixer: Combines the Tx signal and the Rx signal
Digital signal processer (DSP): Performs the calculation

<Detection principles>
(1) Transmitted wave generation: The synthesizer generates transmitted waves in the milli-wave band.
(2) Milli-wave emission: The transmitted waves are continuously emitted from the Tx antenna toward the target.
(3) Reflected wave reception: The Rx antenna receives the reflected waves returned from the target.
(4) Calculation: The mixer combines the transmitted waves and the reflected waves. An A/D converter converts the combined waves into a digital signal. The DSP then performs the calculation to determine the target's distance, speed, angle, and other parameters.

4. mmWave Radar Usage Examples

The FMCW mmWave radar described in section 3 is utilized in many fields. Here, we will explain their usage scenarios and the functions they support by taking automobiles, industrial robots, and drones as examples (Table 3).

Table 3: Application examples of mmWave radar
ApplicationMain usage
scenarios
Frequency
band used
Detected
objects
Functions
supported
AutomobilesVehicle surroundings
monitoring
(front, rear, sides)
In-vehicle monitoring
76 to 81 GHz band
(outside the vehicle)
60 GHz band
(inside the vehicle)
・Obstacles,
 other vehicles
・Condition of
 driver/passenger(s)
・Detection of
 passenger(s) left
 behind
・Automatic braking
・Lane keeping assist
・Contribution to the
 realization of Level
 2 autonomous
 driving
・Improved safety
Industrial
robots
Robot arms
Autonomous mobile
robots (AMRs)
Mainly 60 GHz band/
76 to 81 GHz band
・Distance to people
 and objects
・Speed, angle
・Surrounding
 obstacles
・Avoidance of
 contact with
 people
・Arm movement
 control/stoppage
・Safe autonomous
 traveling
DronesFlying in populated
areas
Mainly 60 GHz band/
76 to 81 GHz band
・Distance to the
 ground
・Pillars, walls
・Power lines, wires,
 antennas
・Obstacle detection
 less likely to be
 affected by the
 weather
・Safe flying in
 populated areas

mmWave radar detects obstacles and other vehicles around a vehicle. This enables functions such as automatic braking and lane keeping assist. Accordingly, mmWave radar is said to be essential for realizing Level 2 autonomous driving (partially automated driving). Furthermore, monitoring the condition of drivers and passengers and monitoring whether passengers have been left behind are attracting attention as indispensable functions for enhancing safety.

Equipping industrial robot arms with mmWave radars makes it possible to detect the distance between the arm and people or objects, as well as providing speed and angle data. This allows predetermined actions, such as stopping the arm's movement, to be performed. In addition, for example, autonomous mobile robots (AMRs) can travel while avoiding obstacles such as shelves, walls, people, and various industrial equipment.

Drones, especially those flying over populated areas, required a high level of safety. Using mmWave radar to detect the flight path of a drone makes it possible to detect not only the distance from the ground but also pillars and walls, as well as power lines, telephone lines, aerial antenna wires, and other obstacles, regardless of the weather conditions. This enables safe flying in populated areas.

Image 1 of mmWave Radar Usage Examples
Image 2 of mmWave Radar Usage Examples

5. Expansion of mmWave Radar into Safety Technology: Euro NCAP Initiative

mmWave radar is being utilized in a variety of fields. In recent years, Euro NCAP*5, which is involved in automobile safety performance assessments in Europe, has set out to strengthen collision safety testing. This has led to attention being paid to the utilization of mmWave radar in cabin monitoring systems that enhance in-vehicle safety.

*5 The European New Car Assessment Programme (Euro NCAP) is an independent organization that assesses and publishes information regarding the safety of new cars sold in Europe. The organization conducts tests to rate advanced safety technologies such those involved in collision safety and pedestrian protection. This information serves as a guide for consumers when choosing a car. The NCAP also has a presence in other countries, while the U.S. has the IHS rating and Japan has the JNCAP.

In 2023, Euro NCAP announced new assessment criteria. In addition to technology that deploys airbags according to the passenger's physique and detection of the usage of seatbelts, a function to detect whether children have been left in the vehicle has been added to the assessment criteria. The aim of the latter is to prevent heatstroke accidents, which have been increasing in number in recent years and are caused by children being left inside vehicles. To meet these requirements, a cabin monitoring system that assesses the conditions inside the vehicle is considered essential.

A cabin monitoring system is a mechanism that uses sensors inside a vehicle to monitor the condition of the driver and other occupants. It then activates the brakes and/or an alarm if necessary. The mechanism consists of a Driver Monitoring System (DMS) that checks the driver's physical condition and level of attention and an Occupant Monitoring System (OMS) that assesses the position and movement of the occupants. Cameras have been widely used as sensors. However, there are many situations that are difficult to detect with cameras alone. They include cases in which a baby is in a rear-facing child seat or an occupant is wrapped in a blanket, and whether a seatbelt is being used.

In this context, mmWave radar is considered a promising device (sensor) to complement or replace cameras. mmWave radar can penetrate fabric and the backs of seats. Therefore, it is capable of detecting objects that cannot be seen by cameras. Moreover, it can capture even minute movements. This also allows it to detect subtle biological changes such as heartbeats and respiration. These characteristics mean that mmWave radar is expected to significantly contribute to improving DMS and OMS functions in cabin monitoring systems and to boost compliance with the new safety criteria required by Euro NCAP.

6. Future of mmWave Radar: Sensor Fusion

mmWave radar is a device - a sensor - with outstanding detection capabilities. However, to meet the diverse detection needs of the future, sensor fusion will be crucial. This sensor fusion combines multiple sensors such as ultrasonic sensors, infrared sensors, and cameras, as well as mmWave radar.
Sensor fusion is a technology that integrates data from multiple sensors to acquire information that cannot be obtained with a single sensor. For instance, combining a mmWave radar with an image sensor makes it possible to acquire information about the driver's fatigue and attention levels not only from their bodily movements but also their eye movements and facial expressions. It is then possible to issue alerts as necessary.
In the future, sensor fusion centered on mmWave radar is expected to be a technology that greatly improves surrounding environment recognition, safety, and reliability, not only in automobiles but also industrial robots, drones, and various forms of mobility.

Other Links

Related products

Related articles