Main image of Sensing Using LF Communication to Improve the Safe Traveling Performance of Autonomous Mobile Robots (AMRs)

Sensing Using LF Communication to Improve the Safe Traveling Performance of Autonomous Mobile Robots (AMRs)

In recent years, transportation robots are increasingly being introduced in logistics warehouses and manufacturing sites. There is therefore a growing need for automation in which the robot itself determines the optimal path and then transports its cargo. Autonomous mobile robots (AMRs) have become increasingly widespread in response to such demand. In this article, we summarize the differences between conventional transportation robots and AMRs. We also explain the effectiveness of sensing using LF communication to address issues facing AMRs, such as sensor malfunctions and missed detections caused by blind spots.

1. What Are AMRs? Transportation Vehicles That Utilize Various Sensors and Wireless Technologies to Self-drive

1.1 Features of AMRs

AMRs are highly autonomous automatic transportation robots. They are garnering particular attention at logistics warehouses and factories where there is a need to eliminate labor shortages and improve work efficiency. The main features of AMRs are as follows.

  • Equipped with diverse sensors to comprehensively acquire information about their environment:
    AMRs are equipped with many sensors. These include LiDAR sensors, cameras, encoders that detect the movement distance and the angle of rotation, and gyro sensors that detect acceleration. AMRs then use the information from these sensors to grasp their surroundings with a high degree of accuracy.
  • Estimate own location and generate maps using simultaneous localization and mapping (SLAM):
    AMRs use information from the aforementioned sensors to generate maps of their environment while estimating their own position. This allows them to recognize the surrounding environment and update their information on it.
  • Flexibly set traveling routes using software:
    It is possible to define traveling routes and behavior via software. This means it is also possible to flexibly respond to changes in the cargo and equipment layout.
  • Coordinate and perform operation management using wireless communication:
    AMRs exchange location information, operating status, and control commands with management systems and other AMRs via Wi-Fi, local 5G, and other communication methods. This realizes operational management, collaborative operation, and improved safety.

1.2 Traveling Methods of AMRs and Conventional AGV Transportation Robots: Self-navigation and Path Guide

Transportation robots have conventionally been called automatic transportation robots, unmanned transportation vehicles, or automatic guided vehicles (AGVs). The traveling route, speed, and stopping positions of AGVs were guided by guidance media (magnetic tape, optical reflective tape, electromagnetic inductance cables, etc.). On the other hand, as mentioned above, AMRs autonomously plan and modify their paths, and move and stop accordingly. We have classified the traveling methods of transportation robots into three types: path guide (AGVs), self-navigation (AMRs), and target guided (example: following a person or cart)*1. We have summarized the differences between these methods in Table 1. AMRs do not require guidance media. This is therefore expected to reduce the operational burden related to the paths they take.

*1 There is a view which considers AGVs that are capable of self-navigating to be AMRs. However, we distinguish here between AGVs and AMRs based on the contrast between the path guide and self-navigation methods.

Image of AGV
AGVs travel alongside the guidance media in the path guide method
Image of AMR
AMRs self-navigate using information from various sensors and management systems
Table 1: Comparison of Transportation Robots with Each Traveling Method

Comparison
Item

Path Guide
(AGVs)

Self-navigation
(AMRs)

Target Guided

Traveling
mechanism

Travels according to
guidance media set up
along the traveling route.

Self-navigates while determining
and modifying its path.
It achieves this by recognizing
its surroundings with LiDAR
sensors, cameras, and other
technologies, and then
estimating its own location and
creating a map using SLAM and
other methods.

Detects the target it will
follow with cameras and other
technologies and then travels
in accordance with the
movements of that target.

Onboard
technologies
(traveling)

Requires guidance media.
Magnetic tape and optical
tape are easy to install.
However, electromagnetic
induction cables require
construction work, such as
burying the cables under
the floor.

Does not require guidance media.
It can flexibly modify its route
by making software-controlled
adjustments.
Requires map and parameter
settings.

Guidance media is not required.
The focus is on the placement
and management of the targets
and tags to be followed.

Onboard
technologies
(sensors)

Guidance media detection
sensors (magnetic and
optical reflective),
guidance media (tape,
cables)

LiDAR sensors, cameras,
accelerometers/gyro sensors,
etc.

Cameras, proximity sensors,
RFID tags

Operation

Dependent on guidance
media. Therefore, the
traveling path and
stopping positions are
fixed and flexibility is low.

It is possible to flexibly modify
the traveling range and path by
updating the software and maps.

Dependent on the targets to
be followed. Therefore, the
degree of route freedom is high,
but behavior is unstable when
it loses the target.

Applications

Routine transportation,
regular transportation
between lines, etc.
(regular transportation
in factories)

Flexible transportation in
warehouses and manufacturing
lines, autonomous transportation
in complex sites

Picking*2 support, convoy
transportation, auxiliary
transportation tailored to
people

*2 Picking: This refers to the task to retrieve and collect products from shelves based on shipping instructions in logistics warehouses and elsewhere

2. AMR Issues: Malfunctions, Collisions, Stop Positioning and Communication Errors

Self-navigating AMRs that safely travel by determining their own traveling routes and avoiding obstacles while detecting people have many advantages. However, interference with traveling still occurs even if using LiDAR sensors, cameras, other optical sensors, and SLAM. Furthermore, there have been many cases in which these problems materialize only after AMRs are introduced. Below, we discuss the main issues facing AMRs.

Sensor (LiDAR and Camera) Malfunctions

The LiDAR sensors and cameras installed on AMRs are capable of highly accurate sensing. However, they sometimes malfunction.
LiDAR can be subject to false reflections from highly reflective glass and shiny metal. It also has difficulty detecting objects with low reflectance. Moreover, smoke, water vapor, and similar can cause false detections. When multiple LiDAR sensors are present in the same space, mutual interference between laser signals can also lead to oversights and false detections.
On the other hand, although cameras are capable of recognition based on image information, they are extremely dependent on the lighting environment. If the light receiving unit becomes saturated (overexposed) due to strong direct light or light sources such as welding, image information may be lost and this may temporarily make detection impossible. Conversely, in dark places, insufficient light reception increases noise, which lowers the recognition accuracy. In addition, reflections from glass and metal surfaces, as well as things like smoke and water vapor, can cause misrecognition.

Collisions with Obstacles and People

LiDAR sensors, which use lasers, and cameras can only detect objects within a clear line of sight. Therefore, they may not be able to detect objects and people hidden from view. Accordingly, these sensors alone cannot detect all obstacles in areas with many blind spots such as those with sharp corners and narrow aisles. That means the robots may collide with cargo and equipment. Furthermore, it might not be possible to detect people in blind spots in areas where people frequently come and go, which could lead to collisions.

Stop Positioning and Boundary Management

Ensuring accuracy and reliability is an issue in AMR stop positioning and boundary management. Measurement errors from LiDAR sensors, cameras, and various other sensors, as well as estimation errors in SLAM and calibration discrepancies between sensors may lead to deviations in the stopping position. Sloping and uneven floors also reduce detection accuracy. As a result, AMRs face issues performing operations that require accuracy at the level of a few centimeters, such as WPT,*3 and in determining the boundaries of restricted zones.

*3 WPT: This is the abbreviation for wireless power transfer. WPT is also known as wireless power supply, and wireless power transmission. It is a system that supplies power to electronic devices without connecting cables.

Communication Errors and Loss of Control

AMRs use SLAM, which allows them to simultaneously estimate their own position and generate maps of their environment, in order to grasp their surroundings and then autonomously determine their traveling route. They receive transportation instructions from a management system while traveling and then move. Therefore, wireless communication with the management system plays an important role.
However, various equipment in manufacturing and other processes can generate electromagnetic noise and wireless signals. Such interference and communication errors can cause unstable communication between the AMR and the management system. This can result in the occurrence of problems such as operational shutdowns and loss of control of the main body.

3. Features of Sensing Using LF Communication

LF is the abbreviation for low frequency. It refers to the frequency band between 30 kHz and 300 kHz. LF communication is a wireless technology that uses this frequency band (LF band). Specifically, LF communication uses frequencies below 135 kHz in the LF band. Sensing is then achieved by communicating with a magnetic field between the transmitting LF antenna and the receiving LF antenna or a radio frequency identification (RFID) tag.

Sensing using this LF communication (hereinafter referred to as "LF sensing") has the following features.

  • Distance measurement is possible:
    Magnetic fields are less affected by reflection and diffraction than radio waves of several hundred MHz. Setting up evenly spaced communication areas around LF antennas makes it possible to measure the distance between the transmitter and receiver by measuring the strength of the magnetic field.
  • High position and distance measurement accuracy:
    The typical detection range of LF communication is short, from a few centimeters to a maximum of five meters. Nevertheless, it has high accuracy, with errors of just a few centimeters when measuring position and distance. There is also almost no variation in the distance measurement values. Accordingly, the results are extremely stable.
  • Less affected by human bodies and water:
    LF sensing uses magnetic fields. For that reason, it is less affected by human bodies and water.
  • Less affected by reflections from metal:
    LF communication is less affected by reflections from metal compared to high-frequency communication methods. Accordingly, there is less multipath interference caused by reflections.

LF communication may be a promising option to solve the issues faced by AMRs that we outlined in section 2: sensor malfunctions, collisions with obstacles and people, and stop positioning and boundary management. Below, we describe how LF communication helps to solve each of these issues.

4. Contribution of LF Sensing to AMR Issues

4.1 Malfunctions

We have shown that the LiDAR sensors and cameras of AMRs sometimes malfunction due to environmental factors (reflections from glass and metal, smoke and water vapor, strong light or dark places, etc.) (refer to section 2). Nevertheless, as we explained in section 3, LF sensing uses magnetic fields. Therefore, it is not affected by strong light or dark places. It can also detect objects with low reflectance. Even in settings where LiDAR sensors and cameras struggle, including environments with smoke and water vapor, LF sensing has the potential to effectively complement the unhindered travel of AMRs.

4.2 Detection of Obstacles and People Hidden from View

We have shown that AMRs face a risk of collision (refer to section 2). However, LF sensing uses magnetic fields, which can easily reach even behind obstacles. This means that even obstacles and people in blind spots created by equipment, walls, and other objects can be detected by LF sensing despite being difficult to detect with LiDAR sensors and cameras.

4.3 Stop Positioning and Boundary Management

Position deviations caused by LiDAR sensor and camera measurement errors, SLAM estimation errors, sensor calibration offset, floor inclines, and other issues make it difficult to ensure accuracy at the level of a few centimeters for stopping positions and to determine restricted zone boundaries (refer to section 2).
Plugging in and unplugging cables for charging is not required with WPT. However, it is still necessary to guide AMRs to locations where they can be supplied power. The position and distance measurement accuracy of LF sensing is high at just a few centimeters. It is therefore expected to enable highly precise guidance to AMR power supply locations and accurate determination of restricted zone boundaries.

Image of Stop Positioning
Supports highly precise guidance to power supply locations
Image of Boundary Management
Determines the boundaries of restricted zones with high accuracy

5. Effective Utilization of LF Sensing in AMRs

AMRs are transportation robots equipped with advanced sensor technologies. Safe traveling and operation are important points when considering the usefulness of AMRs in the field. Moreover, it is essential to consider user perspectives, such as operability, safety, and maintainability. Accordingly, it is important to incorporate the opinions of those in the field and to confirm them through trials and other methods when introducing AMRs into the field. Given this background, it is expected that LF sensing will contribute to solving the issues directly facing AMRs in the field.

Other Links

Related products

Related articles